i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

709 次查看
oobin
Contributor I

Dear Experts

I am working @ i.mx53 serires project, OS is windows embedded compact 7 (winec7).


There are two audio output can be utilized in i.mx53 platform.
One is AUDIO_SGTL5000, the other one is SPDIF(through HDMI).
When playing audio, The audio output always comes form AUDIO_SGTL5000.
I must remove AUDIO_SGTL5000 driver to enable SPDIF out.

Some questions:

1) Can I change audio selection from AUDIO_SGTL5000 to SPDIF when playing audio if both driver exist ?

2) Can AUDIO_SGTL5000 and SPDIF both output audio at the same time ?

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数