i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

708 Views
oobin
Contributor I

Dear Experts

I am working @ i.mx53 serires project, OS is windows embedded compact 7 (winec7).


There are two audio output can be utilized in i.mx53 platform.
One is AUDIO_SGTL5000, the other one is SPDIF(through HDMI).
When playing audio, The audio output always comes form AUDIO_SGTL5000.
I must remove AUDIO_SGTL5000 driver to enable SPDIF out.

Some questions:

1) Can I change audio selection from AUDIO_SGTL5000 to SPDIF when playing audio if both driver exist ?

2) Can AUDIO_SGTL5000 and SPDIF both output audio at the same time ?

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies