We got patch from support case: #00266485, but seems still OOM after apply patch.
Previous report at https://community.nxp.com/thread/528002
We lower the memory to 560M for Linux for decrease the time of duplicate issue.
vi ~/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland/weston_5.0.0.imx.bb
Add below
SRC_URI_append = "\
file://0004-Compositor-weston-memory-leak-when-set-size-value-in.patch \
"
cp ~/0001-Compositor-weston-memory-leak-when-set-size-value-in.patch \
~/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland/weston/0004-Compositor-weston-memory-leak-when-set-size-value-in.patch
cd ~/yocto/build
bitbake -c clean weston
bitbake fsl-image-validation-imx
Solved! Go to Solution.
Hi Igor
Is it possible to have the fix attached to this post or can also send to my email?
I want to see if it fix an issue we see on our devices as well.
Thank you.
I also encountered the same problem. How did you finally solve it?
Hi m.c.
solution was sent via mail.
Best regards
igor
I also encountered the same problem with gpu in imx8mm, can you give me the relevant path?
hufan105@163.com
I saw it and test it on my own, seems issue has been fixed. Once customer confirm, will close this issue. Thank you for your support.
Hi m.c.
I will recheck and update.
Best regards
igor