Hello,
From the discussion forms, I can see that the i.MX6 requires a 5V USB VBUS signal. I would like to know if this requirement is still valid with a i.MX8 processor. Data sheet Table 10 (page 18) gives valid signal for VBUS as 0.8 to 3.6V. Could this be connected to 3.3V?
From the data sheet section 3.9.14.1 it states "Each USBx_VBUS pin must be isolated by and external 30K 1% precision resistor." Does this apply when connecting to the same 3.3V source as used to feed VDD_USB_3P3?
What is your suggested method of connecting USBx_VBUS using a 3.3V supply? I would like to connect it to 3.3V though a 4.75K resistor.
Thanks,
Doug
已解决! 转到解答。