i.MX8 USB VBUS voltage

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX8 USB VBUS voltage

Jump to solution
818 Views
plymale_3
Contributor IV

Hello,

From the discussion forms, I can see that the i.MX6 requires a 5V USB VBUS signal.  I would like to know if this requirement is still valid with a i.MX8 processor.  Data sheet Table 10 (page 18) gives valid signal for VBUS as 0.8 to 3.6V.  Could this be connected to 3.3V?

From the data sheet section 3.9.14.1 it states "Each USBx_VBUS pin must be isolated by and external 30K 1% precision resistor."  Does this apply when connecting to the same 3.3V source as used to feed VDD_USB_3P3?

What is your suggested method of connecting USBx_VBUS using a 3.3V supply?  I would like to connect it to 3.3V though a 4.75K resistor.

Thanks,

Doug

 

Tags (1)
0 Kudos
1 Solution
798 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @plymale_3 

See below, please!

weidong_sun_0-1619051565754.png

Have a nice day!

B.R,

weidong

View solution in original post

3 Replies
777 Views
plymale_3
Contributor IV

Thank you weidong!

0 Kudos
799 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @plymale_3 

See below, please!

weidong_sun_0-1619051565754.png

Have a nice day!

B.R,

weidong

597 Views
musadjan_alim
Contributor II

thanks.

0 Kudos