i.MX8 USB VBUS voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 USB VBUS voltage

ソリューションへジャンプ
7,864件の閲覧回数
plymale_3
Contributor V

Hello,

From the discussion forms, I can see that the i.MX6 requires a 5V USB VBUS signal.  I would like to know if this requirement is still valid with a i.MX8 processor.  Data sheet Table 10 (page 18) gives valid signal for VBUS as 0.8 to 3.6V.  Could this be connected to 3.3V?

From the data sheet section 3.9.14.1 it states "Each USBx_VBUS pin must be isolated by and external 30K 1% precision resistor."  Does this apply when connecting to the same 3.3V source as used to feed VDD_USB_3P3?

What is your suggested method of connecting USBx_VBUS using a 3.3V supply?  I would like to connect it to 3.3V though a 4.75K resistor.

Thanks,

Doug

 

タグ(1)
0 件の賞賛
返信
1 解決策
7,844件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @plymale_3 

See below, please!

weidong_sun_0-1619051565754.png

Have a nice day!

B.R,

weidong

元の投稿で解決策を見る

4 返答(返信)
7,823件の閲覧回数
plymale_3
Contributor V

Thank you weidong!

0 件の賞賛
返信
7,845件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @plymale_3 

See below, please!

weidong_sun_0-1619051565754.png

Have a nice day!

B.R,

weidong

2,724件の閲覧回数
hamzaatifi
Contributor III

Hello @weidong_sun 

I found this reference design for the i.MX8 series, which shows that the USBx_VBUS pin has an internal 60 kΩ pull-down resistor.

Could you please confirm whether the i.MX93 has a similar pulldown resistor on the USBx_VBUS pin?

Thank you in advance!

Best regards,

Hamza

タグ(1)
0 件の賞賛
返信
7,643件の閲覧回数
Musadjan
Contributor III

thanks.

0 件の賞賛
返信