Hello everyone, I am trying to secure boot in i.MX6UL G2 - for not only signed second stage bootloader (SPL). Here is the problem:
While executing hab_status in u-boot command prompt I am getting the following log:
MX6UL_VAR_DART(mmc)==> hab_status
Secure boot disabled
prefetch abort
pc : [<69722070>] lr : [<9ff712ed>]
reloc pc : [<50fb2070>] lr : [<878012ed>]
sp : 9ef6fcc0 ip : 9ffa37b8 fp : 00000001
r10: 9ffa4d98 r9 : 9ef6feb8 r8 : 9ef8b928
r7 : 9ff71361 r6 : 00000000 r5 : 6c41202e r4 : 6972206c
r3 : 9ff85cd1 r2 : 020200b4 r1 : 9ef6fccc r0 : 9ef6fcc8
Flags: nzCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
How I build the u-boot: (SPL and u-boot.img)
git clone https://github.com/varigit/uboot-imx
git checkout imx_v2015.10_dart_6ul_var1
add to include/configs/mx6ul_var_dart.h the following defines:
#define CONFIG_SECURE_BOOT
#define CONFIG_SYS_FSL_SEC_COMPAT 4 /* HAB version */
#define CONFIG_FSL_CAAM
#define CONFIG_CMD_DEKBLOB
#define CONFIG_SYS_FSL_SEC_LE
#define CONFIG_FAT_WRITE
make -j8 ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi- mrproper
make ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi- mx6ul_var_dart_mmc_defconfig
make -j8 ARCH=arm CROSS_COMPILE=arm-poky-linux-gnueabi-
Generate the PKI according with the AN4581
Program the fuses using fuse prog
Device is not closed
Sign using CSF:
[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = ANY
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS
Engine = CAAM
[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install CSFK]
File = "../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate CSF]
#[Unlock]
#Engine = CAAM
#Features = RNG
[Install Key]
Verification index = 0
Target Index = 2
File= "../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate Data]
Verification index = 2
Blocks = 0x877fb000 0x0 0xc00 "./SPL"
What may cause the prefetch abort ?
Why the hab events did not appear?
Thanks,
Robert
~
Hi,
in hab.h define HAB_RVT_BASE should evaluate to 0x00000100 (not 0x00000094)
Hi,
I solve this problem.
Very useful is to compile u-boot (in fact SPL): make SPL V=1 - because we get HAB Blocks info. This info goes to Block in CSF.
There is also a mistake in one define in hab.c - simply the i.MX6ul is not handled
Hello,
0x877fb000 address is used in the CSF - is this correct ?
IS DRAM area properly initialized and working ?
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------