i.MX6UL ENET1 (with DP83848 PHY) is not working in Uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL ENET1 (with DP83848 PHY) is not working in Uboot

884 次查看
kaneshi
Contributor I

Hi all:

The ethernet PHY of my new board is DP83848J, and I changed mx6ul_14x14_evk.h 

pastedImage_1.png

rebuild the uboot. When I download the uboot mirror to the board,the following error is displayed.

pastedImage_26.png

Anyone have any suggestions on what might be wrong or what next to check to get Ethernet working in uboot?

标签 (2)
0 项奖励
回复
1 回复

511 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kane

for error FEC1 address not set one can check

uboot env parameters, like setenv ethprime, setenv ethact, setenv ethaddr.

Can u-boot support more than one ethernet port? - Stack Overflow 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复