Hello Freescale Community,
I thought I had successfully compiled and ported the uboot and kernel along with file system onto an SD card (2 partitions 1 for the bootloader and kernel the other for the fs).
However upon trying to test on the i.MX6SL EVK board through SD2 I found that the board does not boot.
Swapping out to the original MX6LEVK LCD ANDROID r12.10.02 SD card resulted in a non-response as well.
My workstation and Terra Term both still detected connectivity to the board, but there was no boot splash.
Wanting to test the functionality of the board I attempted to run the DDR Stress Tester 1.03 provided by Freescale and found that to still function.
As shown below:
******************************
DDR Stress Test (1.0.3) for MX6SL
Build: Jun 25 2014, 12:09:06
Freescale Semiconductor, Inc.
******************************
=======DDR configuration==========
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 8
Row size: 14, col size: 10
Both chip select CSD0 and CSD1 are used
Density per chip select: 512MB
==================================
What ARM core speed would you like to run?
Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz
ARM set to 1GHz
Please select the DDR density per CHANNEL (in bytes) on the board
Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6
for 32MB
Note, if there are two chip selects per channel, then input the combined densit
y of
both chip selects per channel
DDR density selected (MB): 1024
Calibration will run at DDR frequency 400MHz. Type 'y' to continue.
If you want to run at other DDR frequency. Type 'n'
DDR Freq: 396 MHz
Would you like to run the read/write calibration? (y/n)
Note: Array result[] holds the DRAM test result of each byte.
0: test pass. 1: test fail
4 bits respresent the result of 1 byte.
result 0001:byte 0 fail.
result 0011:byte 0, 1 fail.
Starting Read calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
....
MMDC0 MPRDDLCTL = 0x40404046
Starting Write calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
....
MMDC0 MPWRDLCTL = 0x3630342E
MMDC registers updated from calibration
Read calibration
MPRDDLCTL PHY0 (0x021b0848) = 0x40404046
Write calibration
MPWRDLCTL PHY0 (0x021b0850) = 0x3630342E
The DDR stress test can run with an incrementing frequency or at a static freq
To run at a static freq, simply set the start freq and end freq to the same valu
e
Would you like to run the DDR Stress Test (y/n)?
Enter desired START freq (135 to 672 MHz), then hit enter.
Note: DDR3 minimum is ~333MHz, do not recommend to go too much below this.
396
The freq you entered was: 396
Enter desired END freq (135 to 672 MHz), then hit enter.
Make sure this is equal to or greater than start freq
396
The freq you entered was: 396
Beginning stress test
loop: 1
DDR Freq: 396 MHz
t0.1: data is addr test
t0: memcpy11 SSN test
t1: memcpy8 SSN test
t2: byte-wise SSN test
t3: memcpy11 random pattern test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test
=====================================================
Is there anything obvious as to why the board seems to be not booting from SD2?
Any feedback would be appreciated.
Tae Kim
Please try memory test program with UART logging in order to check
UART-to-USB channel of the EVK.
i.MX6 DDR Stress Test Tool V1.0.3
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------