iMX6Dual : About the DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE for DDR3L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Dual : About the DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE for DDR3L

Jump to solution
539 Views
koichisakagami
Contributor II

Dear community,

We hope to know the DDR_SEL setting of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register.
We know that the register should be set according to description in RM:


  10 : LPDDR2
  11 : DDR3

[Question]


When we use the DDR3L ,
Which setting should we use ,"10" or "00"
on IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE : DDR_SEL ?

Best Regards,
Koichi Sakagami

0 Kudos
Reply
1 Solution
429 Views
Yuri
NXP Employee
NXP Employee

Please use DDR_SEL = DDR3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
430 Views
Yuri
NXP Employee
NXP Employee

Please use DDR_SEL = DDR3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply