Hi community,
I have a question about i.MX6SDL specification.
Please see Table 8 in IMX6SDCEC Rev.4.
There is no VDD_SOC_IN specification other than when VPU <= 328MHz.
Actually, i.MX6DQ has two VDD_SOC_IN specs (when 264MHz < VPU <= 352MHz, and VPU <= 264MHz), but i.MX6SDL has only one.
Is there other i.MX6SDL VDD_SOC_IN specs same as i.MX6DQ? (e.g. 328MHz < VPU < xxx MHz)
If there is no other specs, why i.MX6SDL has only one spec for VDD_SOC_IN?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
i.MX6SDL is quite different processor, so its characrestics are different from i.MX6DQ
Latest VDD_SOC_IN specs are given in datasheet, IMX6SDLCEC
there are no other specs. Such specs as "(e.g. 328MHz < VPU < xxx MHz)"
are not needed, since DDR bandwidth limitation (32bit@400MHz vs 64bit@532MHz)
takes into account.
Re: Re: Memory Reserved on i.MX6 for VPU
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
i.MX6SDL is quite different processor, so its characrestics are different from i.MX6DQ
Latest VDD_SOC_IN specs are given in datasheet, IMX6SDLCEC
there are no other specs. Such specs as "(e.g. 328MHz < VPU < xxx MHz)"
are not needed, since DDR bandwidth limitation (32bit@400MHz vs 64bit@532MHz)
takes into account.
Re: Re: Memory Reserved on i.MX6 for VPU
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I understood what is 264MHz of i.MX6DQ VDD_SOC_IN spec.
It is "AXI clock = 528MHz/2" made from MMDC_CH0 in Figure 18-2 in IMX6DQRM Rev.2.
And I found what is 328MHz, it is core clock limitation written in Table 9-7 in IMX6SDLRM Rev.1.
So I understand why there is no i.MX6SDL VDD_SOC_IN spec about 328MHz < VPU.
However, I have a new question.
Please see Table 9-7 in IMX6DQRM Rev.2, it says the VPU core clock is up to 264MHz.
But the VDD_SOC_IN spec of i.MX6DQ is defined about VPU < 264MHz in Table 6 in IMX6DQCEC Rev.3.
Why is this defined? Is there a case that VPU is used with over 264MHz?
Best Regards,
Satoshi Shimoda
Hi Satoshi
I am afraid I could not fully understand you.
Table 9-7 gives generic VPU description, while
datasheets give specific (different for each processor)
characteristics. You can look at both i.MX6SDL and i.MX6QD
datasheets - they show VPU frequencies. They are different,
since processors are different.
Best regards
igor