i.MX6SDL HDMI supported audio format.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6SDL HDMI supported audio format.

跳至解决方案
1,351 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL HDMI.

We want to confirm the audio format i.MX6SDL HDMI supports.

According to reference manual (IMX6SDLRM Rev.1), I understood i.MX6SDL HDMI supports the following format.

Sample rate: up to 192 kHz

L-PCM bit rate : 16, 24 bits

Then, how about L-PCM 20 bits?

Is it not supported by i.MX6SDL HDMI?

Best Regards,

Satoshi Shimoda

标签 (3)
标记 (1)
0 项奖励
回复
1 解答
980 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes you are right. One will have to convert it to

supported (16, 24 bits) format.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
981 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes you are right. One will have to convert it to

supported (16, 24 bits) format.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
980 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

I understood the hardware supported format.

Then, I want to know the software supported format by BSP also.

I checked Linux reference manual of some revision (L3.0.35, L3.10.17, L3.10.53, and L3.14.28), and there is no description about 24 bits audio in these reference manual even though there is the description about 16 bits audio.

And in source codes (imx-hdmi-dma.c) of these revision, 24 bits audio seems to be not supported.

So I believe 24 bits format by software, is this correct?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
980 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I would suggest to create new thread for this question.

Thanks and Best regards

igor

0 项奖励
回复
980 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

OK, I will create a new thread, thank you.

Best Regards,

Satoshi Shimoda

0 项奖励
回复