i.MX6SDL HDMI supported audio format.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL HDMI supported audio format.

ソリューションへジャンプ
1,349件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL HDMI.

We want to confirm the audio format i.MX6SDL HDMI supports.

According to reference manual (IMX6SDLRM Rev.1), I understood i.MX6SDL HDMI supports the following format.

Sample rate: up to 192 kHz

L-PCM bit rate : 16, 24 bits

Then, how about L-PCM 20 bits?

Is it not supported by i.MX6SDL HDMI?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
978件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes you are right. One will have to convert it to

supported (16, 24 bits) format.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
979件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes you are right. One will have to convert it to

supported (16, 24 bits) format.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
978件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

I understood the hardware supported format.

Then, I want to know the software supported format by BSP also.

I checked Linux reference manual of some revision (L3.0.35, L3.10.17, L3.10.53, and L3.14.28), and there is no description about 24 bits audio in these reference manual even though there is the description about 16 bits audio.

And in source codes (imx-hdmi-dma.c) of these revision, 24 bits audio seems to be not supported.

So I believe 24 bits format by software, is this correct?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
978件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I would suggest to create new thread for this question.

Thanks and Best regards

igor

0 件の賞賛
返信
978件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

OK, I will create a new thread, thank you.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信