i.MX6QP PRE/PRG benefit.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6QP PRE/PRG benefit.

709 次查看
takayuki_ishii
Contributor IV

Hello community,

About new feature of i.MX6QP, it have optimized bus function with PRE/PRG.

Is there a way to see this effect?

like a enable/disable it on demand?

I look forward to hearing from you.

Best regards,

Ishii.

0 项奖励
回复
1 回复

623 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  PRE/PRG feature can help to avoid a potential IPU display under-run in high
loading applications. This feature is "visible" under very heavy loaded system.

Please use IPU driver description in Linux documentation how to configure

the PRE/PRG. In particular look at section 6.3.2 [Image Processing Unit (IPU)]

of "i.MX_Reference_Manual.pdf" in L4.14.78.

https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复