i.MX6Q uSDHC UHS support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q uSDHC UHS support

1,296 Views
NithinkumarN
Contributor II

Hi all,

I'm using i.MX6Q L3.0.35_4.1.0 freescale release in my project.

I need to test UHS-1 Micro SD card in my custom board.

Please let me know is this code release supports this feature?

If not what changes to be done in code as well as board to support this feature.

Thanks and Regards,

Nithin

Labels (2)
0 Kudos
Reply
4 Replies

1,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nithin

I am afraid this release does not support UHS, suggest to try

latest BSP:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,063 Views
NithinkumarN
Contributor II

Hi Igor,

I need to test UHS-1 DDR50 mode in my board.

Is this support also not present in Linux 3.0.35 kernel of L3.0.35_4.1.0 release?

Thanks and Regards,

Nithin

0 Kudos
Reply

1,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nithin

I am afraid not. However it works in latest releases.

Best regards

igor

1,063 Views
NithinkumarN
Contributor II

Hi Igor,

Is there any patch file present for Linux 3.0.35 to support UHS-1 in it.

Thanks and Regards,

Nithin

0 Kudos
Reply