i.MX6Q: What is the maximum DDR throughput?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q: What is the maximum DDR throughput?

1,306件の閲覧回数
Tarek
Senior Contributor I

Hi,

I need to run 16 x 1080p streams and I would like to know if the system can support it or not.

Currently I'm ussing mmdc_prof for monitoring the bandwidth. I can see that the maximum it can reach is around 1046 MB/s but that's not enough. I will need to achieve around 2000 MB/s.

How can I increase the BW capabilities in software?

I'm using the SabreLite board silicon rev 1.0 CPU - 1.0GHZ - 1G RAM

Thanks

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

821件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Hi,

You should be able to reach beyond 1046MB, I'm asking around to find the reason of this limitation. I'll get back to you when I have some feedback.

Michel

0 件の賞賛
返信

821件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Follow  up will be done  in the  https://community.freescale.com/thread/308750

0 件の賞賛
返信

821件の閲覧回数
LeonardoSandova
Specialist I

FranciscoCarrillo , can you help on this one?

Leo

0 件の賞賛
返信