i.MX6Q: What is the maximum DDR throughput?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q: What is the maximum DDR throughput?

1,247 Views
Tarek
Senior Contributor I

Hi,

I need to run 16 x 1080p streams and I would like to know if the system can support it or not.

Currently I'm ussing mmdc_prof for monitoring the bandwidth. I can see that the maximum it can reach is around 1046 MB/s but that's not enough. I will need to achieve around 2000 MB/s.

How can I increase the BW capabilities in software?

I'm using the SabreLite board silicon rev 1.0 CPU - 1.0GHZ - 1G RAM

Thanks

Labels (3)
0 Kudos
Reply
3 Replies

762 Views
ChucoChe
NXP Employee
NXP Employee

Hi,

You should be able to reach beyond 1046MB, I'm asking around to find the reason of this limitation. I'll get back to you when I have some feedback.

Michel

0 Kudos
Reply

762 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Follow  up will be done  in the  https://community.freescale.com/thread/308750

0 Kudos
Reply

762 Views
LeonardoSandova
Specialist I

FranciscoCarrillo , can you help on this one?

Leo

0 Kudos
Reply