i.MX6Q - Test ttymxc1 and ttymxc2.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q - Test ttymxc1 and ttymxc2.

953 次查看
s-s-n
Contributor I

Hello everyone.

How can I test the ports?

It is impossible not to write or read.

In board-mx6q_var_som.h :

static iomux_v3_cfg_t mx6q_var_som_pads[] = {

  ...

  /* UART1 for debug */

  MX6Q_PAD_CSI0_DAT10__UART1_TXD,

  MX6Q_PAD_CSI0_DAT11__UART1_RXD,

  /* UART2 for for Bluetooth */

  MX6Q_PAD_EIM_D28__UART2_CTS,

  MX6Q_PAD_EIM_D29__UART2_RTS,

  MX6Q_PAD_SD3_DAT4__UART2_RXD,

  MX6Q_PAD_SD3_DAT5__UART2_TXD,

  /* UART3 for RS232 port */

  MX6Q_PAD_EIM_D23__UART3_CTS,

  MX6Q_PAD_EIM_EB3__UART3_RTS,

  MX6Q_PAD_EIM_D25__UART3_RXD,

  MX6Q_PAD_EIM_D24__UART3_TXD,

  ...

}

Tell me what I need to do to test the operation of these ports?

标签 (2)
标记 (4)
0 项奖励
回复
0 回复数