Hi community,
I have a question about i.MX6DQ PoP package.
You know the ball mapping of i.MX6DQ PoP package is different from FCBGA package.
Then, how about pin multiplexing?
Are same sigmals are muxed?
(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi
pin multiplexing for i.MX6DQ PoP package is the same
as for FCBGA package.
>Are same sigmals are muxed?
>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)
yes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
pin multiplexing for i.MX6DQ PoP package is the same
as for FCBGA package.
>Are same sigmals are muxed?
>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)
yes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------