Hi,
I'm in the planning stage of my project, and it seems the i.MX6 SoloX would fit the bill perfectly.
But I would need two things:
- being able to retrieve the clock signal from the PHC on INET1
- (optionally) being able to pilot the the PHC on INET2 from an external clock
From the datasheet 1588_EVENT1OUT and friends seem to do what I want, but I couldn't find some documentation on how to use them, and a google search didn't show anything else than that datasheet. Could somebody helpfully point me at the relevant doc ?
Thanks,
Xav
解決済! 解決策の投稿を見る。
Hi Xavier
one can look at sect.24.6.10 IEEE 1588 functions
i.MX6SX Reference Manual (rev.0 2/2015)
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf
and attached Linux Manual Chapter 46 ENET IEEE-1588 Driver.
software example in imx-test-3.14.28-1.0.0 .. /misc/doc/FSL-UT-IEEE1588-001.txt :
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
IXXAT [Evaluation Kits for IEEE1588]
Best regards
igor
Hi Xavier
one can look at sect.24.6.10 IEEE 1588 functions
i.MX6SX Reference Manual (rev.0 2/2015)
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf
and attached Linux Manual Chapter 46 ENET IEEE-1588 Driver.
software example in imx-test-3.14.28-1.0.0 .. /misc/doc/FSL-UT-IEEE1588-001.txt :
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
IXXAT [Evaluation Kits for IEEE1588]
Best regards
igor
FSL-UT-IEEE1588-001.txt
Run the IXXX stack: ./ptp_main -d -o -m -l -w -z
There is no ./ptp_main executable or source code in imx-test-3.14.28-1.0.0.tar.gz
IXXAT [Evaluation Kits for IEEE1588] This link cannot be downloaded, prompting the following error:
404 - File or directory not found
Thanks Igor, lots to read and it seems everything's in there.