i.MX6 SPDIF 96KHz playback support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 SPDIF 96KHz playback support

1,673 次查看
saurabh206
Senior Contributor III


Hi Community,

BSP 3.14.28.

I am able to get 48KHz, playback using SPDIF out.

96KHz playback is not working. I have not seen any error in SPDIF register.

96KHz playback support is available? Or any modification is required?

标签 (2)
标记 (1)
0 项奖励
回复
5 回复数

1,383 次查看
shanxigjz
Contributor II

Hi  Saurabh,

I am trying to imx6 spdif output to play audio files.

but i can not get it work.

When i play files, it blocked and never return back.

Could you tell me how you get your spdif output playback worked?

Thank you very much.

0 项奖励
回复

1,383 次查看
saurabh206
Senior Contributor III

Hi Gao,

We are able to get 96KHz playback working.

Thanks

Saurabh

0 项奖励
回复

1,383 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

seems s/pdif driver does not support it as described in attached Linux

Manual sect.31.1.3 Software Overview

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,383 次查看
saurabh206
Senior Contributor III

Hi Igor

Thanks for your replay.

Is there any software limitation or hardware limitation?

However Manual mentioned that 96KHz capture support is available.

96KHz , 24 bit is now very generalized audio requirement.

Thanks

Saurabh

0 项奖励
回复

1,383 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

this is driver limitation, not hardware

~igor

0 项奖励
回复