Hi,
in my application I'm using an i.MX6-quad.
I measure the die temperature by:
cat/sys/class/thermal/thermal_zone0/temp.
What is the upper limit I should consider for this value so that the product
works in a safe condition?
Thanks in advance.
Best Regards,
Diego
已解决! 转到解答。
The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The datasheet is located here:
http://www.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
you can check table 4.1.3
The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------