i.MX6 CPU temperature is too high

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 CPU temperature is too high

2,925 Views
petertseng
Contributor IV

Hello,

In our custom board which is designed more closer to i.MX6Q SABRE SD.

When I normally boot into Android 4.3 system and enable stay awake keep for some time.

I get the CPU temperature:

root@sabresd_6dq:/ # cat /sys/class/thermal/thermal_zone0/temp                 

52

When the system does not execute any APK, the CPU temperature has been maintained at 53 ~ 49.

When executed Cactus Player, CPU temperature will be higher than 53.

Is that normal?

Thanks.

Regards,

Peter Tseng

Tags (4)
0 Kudos
Reply
3 Replies

1,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

I think this can be considered as normal since VPU/GPU consumes

quite lot of energy. Some power consumption figures can be found in

below application note

AN4509 i.MX 6Dual/6Quad Power Consumption Measurement

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,064 Views
petertseng
Contributor IV

Hi igor

But, when our system does not execute any APK, the CPU temperature has been maintained at 53 ~ 49.

Is it also normally?

PS: I did not use any heatsink on our i.MX6Q CPU

0 Kudos
Reply

1,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

I think this is normal.

Best regards

igor

0 Kudos
Reply