i.MX6 Boot from SPI - alternative pinmux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Boot from SPI - alternative pinmux

ソリューションへジャンプ
1,199件の閲覧回数
dmitryv
Contributor II

Hello!

I have a question regarding iMX6 boot from SPI flash. If you look to MCIMX6Q-SDB schematics, you will find the following pin connection for SPI NOR flash (only 2 lines as example):

  SPINOR_CLK  --->>> KEY_COL0 [W5] . ALT0 = ECSPI1_CLK

  SPINOR_MISO --->>> KEY_COL1 [U7] . ALT0 = ECSPI1_MISO

However, according to RM "Table 8-25. SPI IOMUX Pin Configuration", or DS "Boot Devices Interfaces Allocation", booting from ECSPI1 is possible if connected to EIM_D17.alt1, EIM_D18.alt1, etc...

Does that mean that MCIMX6Q-SDB is not able to boot from onboard SPI NOR flash?

Or does boot ROM look to alternative pin options as well?

Thank you!

--

Dmitry

ラベル(1)
0 件の賞賛
返信
1 解決策
781件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

you are correct:

from i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf L3.0.35_4.1.0_LINUX_DOCS

Table 7. Known Issues and Workarounds

"Current SD board uses KEY relative PINs as

SPI interface. However, this set of PINs are not

supported by ROM.

Therefore, SPI NOR boot is not supported by Smart Device Board."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
782件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

you are correct:

from i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf L3.0.35_4.1.0_LINUX_DOCS

Table 7. Known Issues and Workarounds

"Current SD board uses KEY relative PINs as

SPI interface. However, this set of PINs are not

supported by ROM.

Therefore, SPI NOR boot is not supported by Smart Device Board."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信