i.MX535 QSB jpeg image Errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX535 QSB jpeg image Errors

3,081 次查看
shanmugamsundar
Contributor IV

hi all,

       I am working in i.mx535qsb board, in that i want to capture the jpeg image format, when i captured the image the header of the image is not coming, for your convenience, i have attached the sample image also, can any one help me,

NOTE:

Camera sensor = ov5640

Board = i.mx535 qsb

Resolution = 1280x720

thanks,

shan

标签 (3)
0 项奖励
回复
12 回复数

2,030 次查看
LeonardoSandova
Specialist I

Hi,

which JPEG encoder are you using?

0 项奖励
回复

2,030 次查看
shanmugamsundar
Contributor IV

hi

i am using jif encoder not jfif

0 项奖励
回复

2,030 次查看
LeonardoSandova
Specialist I

Perhaps the problem is the encoder.  Can you try out other encoder? can you try to encode other format?

Under imx6 platform, I have used GStreamer to capture images, take a look of this document

GStreamer iMX6 image capture

0 项奖励
回复

2,030 次查看
shanmugamsundar
Contributor IV

hi

i tried the command from that document but it shows there is no jpeg enc  in the gstreamer . how can i enable that codec

ERROR:

WARNING: erroneous pipeline: no element "jpegenc"

thanks

shan

0 项奖励
回复

2,030 次查看
LeonardoSandova
Specialist I

Follow this Document to enable the jpegdec

GStreamer iMX6 Image Display

0 项奖励
回复

2,030 次查看
shanmugamsundar
Contributor IV

hi leonardo,

                i have captured the images in jpeg format, the problem is hard ware connection, and do you know the jpeg settings for 5mp resolution or if there any documents kindly share it

Thanks

shan

0 项奖励
回复

2,030 次查看
LeonardoSandova
Specialist I

Hi shanmugamsundar, I did not get your point. what do you mean by 'hard ware connection'? One the image is encoded? can you decode and display on the board? can you do the same on your host machine?

0 项奖励
回复

2,030 次查看
prabhurammuruga
Contributor I

Hi

Leonardo Sandoval Gonzalez,

I am working on iMX 53 and Android 2.3 build,

I need to use the VPU to decode the jpeg image (software decoding works fine but going for VPU decode for better performance)
I had checked the mxc_vpu_test and the config files, there are options for decoding movie formats like MJPG , MPEG etc  in config_dec. But I could not see any options for JPEG decoding ???

So is it possible to use VPU for image file (jpg | bmp | png) decoding efficiently ?

0 项奖励
回复

2,030 次查看
LeonardoSandova
Specialist I

Hi prabhurammurugan,

could you please post the question in a new document? Doing this more people will see it and in case there is no answer, your question is assigned to a specialist.

0 项奖励
回复

2,029 次查看
prabhurammuruga
Contributor I

I have posted as new discussion & below is the link

Jpeg image decoding using VPU on iMX53 running Android 2.3

Thank you,

0 项奖励
回复

2,030 次查看
shanmugamsundar
Contributor IV

hi ,

I am using ipu csi encoder

0 项奖励
回复

2,029 次查看
shanmugamsundar
Contributor IV

hi sorry

       jpeg jfif encoder

0 项奖励
回复