hi all,
I am working in i.mx535qsb board, in that i want to capture the jpeg image format, when i captured the image the header of the image is not coming, for your convenience, i have attached the sample image also, can any one help me,
NOTE:
Camera sensor = ov5640
Board = i.mx535 qsb
Resolution = 1280x720
thanks,
shan
Perhaps the problem is the encoder. Can you try out other encoder? can you try to encode other format?
Under imx6 platform, I have used GStreamer to capture images, take a look of this document
hi
i tried the command from that document but it shows there is no jpeg enc in the gstreamer . how can i enable that codec
ERROR:
WARNING: erroneous pipeline: no element "jpegenc"
thanks
shan
Follow this Document to enable the jpegdec
hi leonardo,
i have captured the images in jpeg format, the problem is hard ware connection, and do you know the jpeg settings for 5mp resolution or if there any documents kindly share it
Thanks
shan
Hi shanmugamsundar, I did not get your point. what do you mean by 'hard ware connection'? One the image is encoded? can you decode and display on the board? can you do the same on your host machine?
Hi
I am working on iMX 53 and Android 2.3 build,
I need to use the VPU to decode the jpeg image (software decoding works fine but going for VPU decode for better performance)
I had checked the mxc_vpu_test and the config files, there are options for decoding movie formats like MJPG , MPEG etc in config_dec. But I could not see any options for JPEG decoding ???
So is it possible to use VPU for image file (jpg | bmp | png) decoding efficiently ?
Hi prabhurammurugan,
could you please post the question in a new document? Doing this more people will see it and in case there is no answer, your question is assigned to a specialist.
I have posted as new discussion & below is the link
Jpeg image decoding using VPU on iMX53 running Android 2.3
Thank you,