Hello Champs,
I need to boot by NOR Flash in muxed at low half bits.
I understand I need to set 00 at BOOT_CFG2[7:6] in OCOTP.
However which addresses are these bits or fuse located?
Best regards,
Nori Shinozaki
Solved! Go to Solution.
Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.
Regards,
Yuri.
BOOT_CFG2[7:6] corresponds OCOTP_CFG3[23:22] .
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yuri,
Thanks,
So I set 00 in OCOTP_CFG3[23:22] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?
Best regards,
Nori Shinozaki
Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.
Regards,
Yuri.
Yuri,
Thank you!
I created a new thread for this question on a different subject, but please ignore it.
Best regards,
Nori Shinozaki