i.MX50: Where is the fuse for Muxed(low half) NOR Flash boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX50: Where is the fuse for Muxed(low half) NOR Flash boot

Jump to solution
811 Views
norishinozaki
Contributor V

Hello Champs,

I need to boot by NOR Flash in muxed at low half bits.

I understand I need to set 00 at BOOT_CFG2[7:6] in OCOTP.

However which addresses are these bits or fuse located?

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
1 Solution
712 Views
Yuri
NXP Employee
NXP Employee

Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.

Regards,

Yuri.

View solution in original post

0 Kudos
4 Replies
712 Views
Yuri
NXP Employee
NXP Employee

BOOT_CFG2[7:6] corresponds OCOTP_CFG3[23:22] .

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
712 Views
norishinozaki
Contributor V

Yuri,

Thanks,

So I set 00 in OCOTP_CFG3[23:22] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?

pastedImage_0.png

Best regards,

Nori Shinozaki

0 Kudos
713 Views
Yuri
NXP Employee
NXP Employee

Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.

Regards,

Yuri.

0 Kudos
712 Views
norishinozaki
Contributor V

Yuri,

Thank you!

I created a new thread for this question on a different subject, but please ignore it.

Best regards,

Nori Shinozaki

0 Kudos