i.MX28 can't run recently u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX28 can't run recently u-boot

738 次查看
GKhan
Contributor I

Yes, just tested and it can't working fine.

Clone u-boot:

git clone https://source.denx.de/u-boot/u-boot

u-boot version 

VERSION = 2022
PATCHLEVEL = 04

Build U-boot as doc u-boot/doc/imx/common/mxs.txt 

make mrproper

make mx28evk_defconfig

make u-boot.sb

Set the jumpers to 0 0 0 0.

Connect USB cable from mx28evk to the host PC.

Power up the board.

sudo ./mxsldr u-boot.sb

Detected: i.MX28

Chip ID:          0x2800

Chip Revision:    0x0001

ROM Version:      0x0101

Protocol Version: 0x0100

and then U-boot has nothing messages come up....

标签 (1)
0 项奖励
回复
0 回复数