Hello,
We did design a board based on the Freescale i.MX28 EVK, we are trying to boot it using the MfgTool which work fine with the EVK. But with our board the boot stop during ROM loader process.
The message I get from the DEBUG UART is :
PowerPrep start initialize power...
Battery Voltage = 0.40V
No battery or bad battery detected!!!.
Disabling battery
voltage measurements./r/nLLLCDec 27 201009:58:45
with the EVK it continue like written below :
PowerPrep start initialize power...
Battery Voltage = 1.18V
No battery or bad battery detected!!!.Disa
bling battery voltage measurements./r/nDec 27
201009:22:42
FRAC 0x92925552
memory type is DDR2
Wait for ddr ready 1power 0x00820616
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
start test memory accress
ddr2 0x40000000
finish simple test
It might be a hardware problem on our board but we did not find any yet. Did somebody had a similar problem or have an idea about what could make the ROM loader stop at this point ?
Any suggestion or ideas how to investigate are welcome.
Thanks by advance
Jean-Marc
You build&deploy it with :
./ltib -m scbuild -p imx-bootlets
./ltib -m scdeploy -p imx-bootlets
You then use the bootstream generated in rootfs/boot/
Thanks Vladan...
I'm now able to modify the bootlet code....What's the next step to use the changed code in my imx28 board?
Vladan Jovanovic said:
./ltib -m prep -p imx-bootlets
They will be in <ltib>/rpm/BUILD/ directory.
./ltib -m prep -p imx-bootlets
They will be in <ltib>/rpm/BUILD/ directory.
Hello,
My problem was inside bootlets during power_prep, by uncomment the #define NO_BATTERY_VOLTAGE_SOURCE in power_prep.c, the operation and automatic voltage measurements are disabled and then it worked. The boot was stopping inside the bootlets, your problem seems to be different. I guesss you see finish simple test then nothing more. It's the kernel which doesn't show any message. I would verify the jump adress, the adress where kernel is copied, also if kernell start but console is not set on the right serial port.
Best regards
Hi Jean-Marc,
We have exact same issue, on our custom board , we dont see any thing after linux_prea.
I have debug print just before jump to KERNEL, after that nothing ??
Any idea on the fix, Will appricate any help.
our ddr part number is W971GG6JB form winbound - 64Mbyte
BR,
RA
Thank you very much for your help Vladan.
I did not know it work this way with the bootlets, by adding some printf I was able to find the problem come from the power rails. It's now working.
Best regards.
This is not ROM loader failure, it's a failure in one of the bootlets that runs at startup to initialize basic system settings (power rails, memory etc.). Add some printfs there to locate the issue (look at boot_prep package in ltib). This probably happens due to differences between your schematic and ref. design, so you have to adjust the bootlets (can be memory timing issue for example)...
br,
Vladan