i.MX28 HAB (High Assurance Boot) for Windows CE6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX28 HAB (High Assurance Boot) for Windows CE6.0

跳至解决方案
1,075 次查看
garylijs
Contributor II

Hi,

I want to construct boot image(sb files) on i.MX28 for Windows CE6.0, but I don't search any doc or tools about the Windows CE6.0 in the freescale website, only there're Linux platform. How can I get these support?

Follow are my questions:

1. How to prepare the unsigned Image ELF file for the firmware that is to be booted by the ROM under Windows CE platform?

2. Sign the image with the code signing tool,which generates one HAB.ELF file . I only find one CST for linux, not for Windows CE6.0. How can I get one CST package for Windows CE?

Thanks,

Gary

标签 (1)
0 项奖励
1 解答
825 次查看
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
5 回复数
825 次查看
garylijs
Contributor II

Nobody knows how to do under Windows CE6???

Who could give me "HAB CST User's Guide" first? Let me study it first.

Thanks,

Gary

0 项奖励
825 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
825 次查看
garylijs
Contributor II

Hi Yuri,

It's only for linux, do you have any CST for windows.

Regards,

Gary

0 项奖励
826 次查看
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

0 项奖励
825 次查看
garylijs
Contributor II

Hi Yuri,

There can only be so, thanks.

Regards,

Gary

0 项奖励