i.MX28 HAB (High Assurance Boot) for Windows CE6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 HAB (High Assurance Boot) for Windows CE6.0

Jump to solution
1,053 Views
garylijs
Contributor II

Hi,

I want to construct boot image(sb files) on i.MX28 for Windows CE6.0, but I don't search any doc or tools about the Windows CE6.0 in the freescale website, only there're Linux platform. How can I get these support?

Follow are my questions:

1. How to prepare the unsigned Image ELF file for the firmware that is to be booted by the ROM under Windows CE platform?

2. Sign the image with the code signing tool,which generates one HAB.ELF file . I only find one CST for linux, not for Windows CE6.0. How can I get one CST package for Windows CE?

Thanks,

Gary

Labels (1)
0 Kudos
1 Solution
803 Views
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

View solution in original post

0 Kudos
5 Replies
803 Views
garylijs
Contributor II

Nobody knows how to do under Windows CE6???

Who could give me "HAB CST User's Guide" first? Let me study it first.

Thanks,

Gary

0 Kudos
803 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
803 Views
garylijs
Contributor II

Hi Yuri,

It's only for linux, do you have any CST for windows.

Regards,

Gary

0 Kudos
804 Views
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

0 Kudos
803 Views
garylijs
Contributor II

Hi Yuri,

There can only be so, thanks.

Regards,

Gary

0 Kudos