i.MX28 HAB (High Assurance Boot) for Windows CE6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28 HAB (High Assurance Boot) for Windows CE6.0

ソリューションへジャンプ
1,270件の閲覧回数
garylijs
Contributor II

Hi,

I want to construct boot image(sb files) on i.MX28 for Windows CE6.0, but I don't search any doc or tools about the Windows CE6.0 in the freescale website, only there're Linux platform. How can I get these support?

Follow are my questions:

1. How to prepare the unsigned Image ELF file for the firmware that is to be booted by the ROM under Windows CE platform?

2. Sign the image with the code signing tool,which generates one HAB.ELF file . I only find one CST for linux, not for Windows CE6.0. How can I get one CST package for Windows CE?

Thanks,

Gary

ラベル(1)
0 件の賞賛
返信
1 解決策
1,020件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,020件の閲覧回数
garylijs
Contributor II

Nobody knows how to do under Windows CE6???

Who could give me "HAB CST User's Guide" first? Let me study it first.

Thanks,

Gary

0 件の賞賛
返信
1,020件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
1,020件の閲覧回数
garylijs
Contributor II

Hi Yuri,

It's only for linux, do you have any CST for windows.

Regards,

Gary

0 件の賞賛
返信
1,021件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Alas, we do not have CST for Windows host. Please use Linux
virtual machine under Windows. The CST "output" is OS-independent.

Regards,
Yuri.

0 件の賞賛
返信
1,020件の閲覧回数
garylijs
Contributor II

Hi Yuri,

There can only be so, thanks.

Regards,

Gary

0 件の賞賛
返信