Hello everyone,
I face some problem about HDMI output.
I connected the LVDS to HDMI adapter to J2, but the display always no signal. I already take one day to survey the solution.
I only find a related solution at https://community.nxp.com/t5/i-MX-Processors/HDMI-Output-in-i-MX-8QuadMax/td-p/1087406
Although the kernel version are a little different, I change the fdt_file to the corresponding file, imx8qm-mek.dtb.
It still doesn't work.
At the end, I try to change the plug. I find something weird.
I can get the output from J7/J8 plug, but i can't get the ouput from J2/J3 plug.
Information about setting
Board: i.MX8 QuadMax MEK
Linux Kernel version:Linux -2.2.0+g5ec03d06f54e #1 SMP PREEMPT Thu Sep 24 06:58:12 UTC 2020 aarch64 aarch64 aarch64 GNU/Linux
Uboot version:- U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5
dts:fdt_file=imx8qm-mek.dtb
Is there new change in imx8qmmek 5.4.47 ?
已解决! 转到解答。
I try the other vision, the situation are the same. It still can't get the output from J2/J3.
Linux imx8qmmek 4.19.35-1.1.0+g0f9917c56d59 #1 SMP PREEMPT Wed Oct 30 13:09:11 UTC 2019 aarch64 aarch64 aarch64 GNU/Linux Linux imx8qmmek 4.14.62-imx_4.14.62_1.0.0_beta+g1907fe4 #1 SMP PREEMPT Tue Oct 16 06:33:37 UTC 2018 aarch64 aarch64 aarch64 GNU/Linux