i.MX 8M Plus IBIS-AMI not supported by Altium

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus IBIS-AMI not supported by Altium

552 Views
Dan1111
Contributor III

Hi,

I'm using MIMX8ML8CVNKZAB in a project and I tried to add the provided i.MX 8M Plus 15x15 IBIS Model (ibis_imx8mp_v2_20201023) to the Altium symbol.

However, Altium Support claim that Altium only supports IBIS specification up to and including 4.0, and that IBIS-AMI was only added to the spec in version 5.0. The i.MX IBIS file is version 6.0.

Can I please have an IBIS version 4.0 file for MIMX8ML8CVNKZAB ?

 

I get the following errors.

  • ERROR - AMI_Version "6.0" is not valid
  • ERROR - Unknown parameter Tx_Rj found as a child of Reserved_Parameters
  • ERROR - Unknown parameter Rx_Dj found as a child of Reserved_Parameters

e.g. there are AMI references in this IBIS V6.0 file.

  • Line 812 : [Model Selector] USB3_RX
  • Line 813 : synopsys_usb3_rx_ami synopsys_usb3_rx_ami
  • Line 814 : synopsys_usb3_rx_ami_jitter synopsys_usb3_rx_ami_jitter

 

Kind regards,
Dan

2 Replies

511 Views
jimmychan
NXP TechSupport
NXP TechSupport

IBIS version 4.0 doesn't support IBIS-AMI model so it is not recommended to use Altium for simulation. Please use professional tools for simulation.

0 Kudos
Reply

499 Views
Dan1111
Contributor III

Thanks Jimmy,

 

Is it possible to export an IBIS V4.0 from whatever tool it was created in?

I don't have access to other tools, and I'm unlikely to be able to gain access during the scope of this project.

0 Kudos
Reply