This Group is to talk and discuss about i.MX6 related topics. The i.MX 6 Series unleashes a scalable multicore platform that includes single-, dual- and quadcore families based on the ARM® Cortex™-A9 architecture for next-generation consumer, industrial and automotive applications.
Hi all,
Now I'm working with MX6Q for cusotmer project, refer to FSL QSB that we have worked out our customer board, the question is we can't boot from SD card directly, could anyone has the success experience to share ? thx
iWave Systems announced the World's first availability of WEC7 BSP on i.MX6 SOM Development Platform besides the existing Linux 3.0.15 & Android ICS 4.0 BSP versions.Please see the below links for more details.
http://imxcommunity.org/group/i-mx6-som-development-platform
Guideline to address sneak current between any i.MX device and unpowered connected peripherals is as follows.
Option 1: While the i.MX device is powered on but connected devices are off, program iMX6 I/O as outputs at a low level.
Option 2: While the i.MX device is powered on but connected devices are off, program iMX6 I/O as inputs with pull-down enabled.