i.MX 6 Series Processors - wall comments

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6 Series Processors - wall comments

1,438件の閲覧回数
DirkBehme
Contributor III

This Group is to talk and discuss about i.MX6 related topics. The i.MX 6 Series unleashes a scalable multicore platform that includes single-, dual- and quadcore families based on the ARM® Cortex™-A9 architecture for next-generation consumer, industrial and automotive applications.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,263件の閲覧回数
Oceanblue
Contributor III

Hi all,

   Now I'm working with MX6Q for cusotmer project, refer to FSL QSB that we have worked out our customer board, the question is we can't boot from SD card directly, could anyone has the success experience to share ? thx

0 件の賞賛
返信

1,263件の閲覧回数
DirkBehme
Contributor III

sachin rai: Regarding the IMX6 Functional spec: As far as I know the i.MX6 spec is still confidential. Please ask you Freescale contact.

0 件の賞賛
返信

1,263件の閲覧回数
sachinrai
Contributor I

Hi All,

Can anyone point me to the IMX6 Functional spec?

I'm interested more on the Hardware implementation and modules present in the IMX apps processor.

 

Thanks!

/Sachin

0 件の賞賛
返信

1,263件の閲覧回数
PradapRaj
Contributor III

iWave Systems announced the World's first availability of WEC7 BSP on i.MX6 SOM Development Platform besides the existing Linux 3.0.15 & Android ICS 4.0 BSP versions.Please see the below links for more details.

http://imxcommunity.org/group/i-mx6-som-development-platform

http://imxcommunity.org/group/i-mx6-som-development-platform/page/iwave-systems-announced-the-availa...

0 件の賞賛
返信

1,263件の閲覧回数
PradapRaj
Contributor III

Quad display demo on i.MX6 CPU with iWave's 'i.MX6 SOM Developement platform' in 'FTF Americars2012' @ pedestal 1112...

http://imxcommunity.org/group/i-mx6-som-development-platform

0 件の賞賛
返信

1,263件の閲覧回数
david_babin
NXP Employee
NXP Employee

Guideline  to address sneak current between any i.MX device and unpowered connected peripherals is as follows.
 
Option 1: While the i.MX device is powered on but connected devices are off, program iMX6 I/O as outputs at a low level.

Option 2: While the i.MX device is powered on but connected devices are off, program iMX6 I/O as inputs with pull-down enabled.

0 件の賞賛
返信