how to set the efuse (OTP) with jtag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to set the efuse (OTP) with jtag

1,568件の閲覧回数
nick76
Contributor I

Hello..

I would like to set efuse(OTP) with Jtag(DS-5) on the IMX6Q custom Board.

is it possible ?

If possible, let me know how to set the value..

Regards,

Nick

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,335件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Seongwoong

one can try to implement attached baremetal sdk example

using jtag scripts, please use Chapter 25 Configuring the OCOTP Driver

pdf document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,335件の閲覧回数
nick76
Contributor I

Thank you.

Our purpose is to live our custom board from SD memory.

- boot mode settings is possible,

- there are no pins (BT_CFG1_0~7, BT_CFG2_0~7,BT_CFG3_0~7, BT_CFG4_0~7) so it is impossible for boot by GPIO.

- there is no otg USB.

Aa a result, we have to live our custom board with JTAG(Dstream)

I don't have the jtag script..

would you explain to me in detail?

The attached file is ref. schematic

Regards,

Nick.

0 件の賞賛
返信