how to add or remove packages from lollipop build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to add or remove packages from lollipop build

552 Views
damienhuang
Contributor IV

I am customising the lollipop image got from boundary for my imx6 board because I don't need any phone, bluetooth & wifi related applications, could someone help to give some directions?

there is "generic_no_telephony.mk", how can I switch to use this mk file for build?

Cheers,

Labels (2)
0 Kudos
Reply
1 Reply

507 Views
b36401
NXP Employee
NXP Employee

You can refer Android User's Guide:

https://www.nxp.com/webapp/Download?colCode=IMX6_L5.1_2.1.0_ANDROID-DOCS

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply