how can I using nfs service on I.mx8m android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can I using nfs service on I.mx8m android

996件の閲覧回数
pjw
Contributor II

Hi, I'm using I.mx8m, and I used Android 8.0 to boot the board. My purpose is to connect to the nfs server from the i.mx8m board using nfs. It was built with nfs in kernel menuconfig to use nfs, but nfs is not available. It says that the device cannot be found when nfs mount.

 

Do I need to make any other settings besides building with nfs in the kernel? Or is nfs not available on Android?

And what should I do to use ssh? It is said that the ssh command does not exist at present.

 

I'd appreciate it if you could let me know some data or answer.

0 件の賞賛
返信
1 返信

987件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

It is not supported since it represents a breach in security.

 

Thank you for your comprehension.

 

BR,

Ivan.

0 件の賞賛
返信