Hi there:
I am now have one i.MX 6Quad SABRE-AI Platform with an Ethernet PHY of BCM89810, and I have bitbaked fsl-image-qt5 , but how can I get the driver of BCM89810?
I also have a MPC5604EKIT,but dont have the driver of BCM89810 too.
How can I get it?
Hi Haining
seems driver is included as part of AVB Stack for IMXAI2ETH-BRC board
Audio Video Bridging Software|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi :
I have another question.
I have finish the yocto project,and bitbake successfully as blow:
MACHINE=imx6qsabreauto source fsl-setup-release.sh -b build-wayland -e wayland | |
bitbake fsl-image-qt5 |
after dd cmd ,it boot up successfully from serial display,but the HDMI has no signal.
Hi guy
I have bought the hardware IMXAI2ETH-BRC board from the NXP website, if I want to get the driver,I must pay for it again?