gstreamer can't play mp4 file on imx8mq-evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gstreamer can't play mp4 file on imx8mq-evk

909件の閲覧回数
quanyang_wang
Contributor II

Hi Experts,

I build a imx-image-multimedia yocto project (imx_6.1.55_2.2.0)  and deploy it to i.mx8mqevk board. I tried to play a mp4 file but it failed with the following error log:

root@imx8mqevk:~# gst-launch-1.0 filesrc location=/wqy/1.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! v4l2h264dec ! autovideosink
Setting pipeline to PAUSED ...

====== V4L2DEC: 1.22.5 build on Oct 19 2023 01:57:00. ======
Pipeline is PREROLLING ...

====== AIUR: 4.8.2 build on Oct 10 2023 02:31:27. ======
Core: MPEG4PARSER_06.21.06 build on Oct 18 2023 10:08:29
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:03:47.458333000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)4096, height=(int)2304, framerate=(fraction)24/1, codec_data=(buffer)01640033ffe1001867640033acb400800090d0
800000030080000018078c195001000468ce0bcb
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:03:47.439455000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)191992, stream-format=(string)raw, codec_data=(buffer)12100000000000000000000000000000
------------------------
WARNING: from element /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0: Delayed linking failed.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.22.5.imx-r0/gst/parse/grammar.y(855): gst_parse_no_more_pads (): /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0:
failed delayed linking some pad of GstAiurDemux named aiurdemux0 to some pad of GstQueue named queue0
^Chandling interrupt.
Interrupt: Stopping pipeline ...
Setting pipeline to NULL ...
Freeing pipeline ...

Is there any suggestion about this error?

 

0 件の賞賛
返信
2 返答(返信)

885件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

That Quicktime pluging is not in the supported list maybe this is the problem.

Regards

0 件の賞賛
返信

864件の閲覧回数
quanyang_wang
Contributor II

Hello,

Thank you for replying.

The command line is picked from Section 7.3.1.2 "Video-only playback" of the Document "i.MX Linux User's Guide".  If Quicktime plugins do not work, are there any plugins that can be used to play mp4 files?

Any suggestion is appreciated.

Thanks,

0 件の賞賛
返信