emwin graphic library with iMXRT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emwin graphic library with iMXRT

901件の閲覧回数
johnot
Contributor I

Hi ,

 

   Is the emwin graphic library with iMXRT freely available?

Is it possible to use emwin graphic library in imxrt based commercial products free of cost?

 

Best regards,

John OT

0 件の賞賛
返信
2 返答(返信)

677件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi John OT,

Yes, the emwin graphic library with iMXRT  is freely available. You can use it.

Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

677件の閲覧回数
johnot
Contributor I

Hi Rita,

 

   Thanks for the quick reply.

 

  Have couple of questions.

  1. We didn't want to use hyper flash, instead we want to use either QSPI or SD card.

  2. Can we use sd card to boot the system and run the emwin gui? Is tools are available to program the SD card from out side and use it in RT board? 

  3. Can we use qspi with emwin gui? Since emwin occupy a bigger amount of memory, is it wise to use QSPI for booting? Is tools are available to program the qspi  with USB/uart  connections with PC?

 

Best regards,

John OT

0 件の賞賛
返信