Hi,
Hi Andrea
one can try "split-mode = <1>;" as ldb driver uses "of_property_read_bool" in linux/drivers/video/fbdev/mxc/ldb.c :
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/video/fbdev/mxc/ldb.c?h=imx_4.1.15...
example of split-mode = <1>; can be found on:
https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts/im...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor, I tried your solution bU I still have problems. It seems my
display in set on a different configuration then Full Color but, as I can
see in the u-Boot environment, lcd_panel is LDB-19201080,if=RGB24 ldb=spl0.
Thank you for helping
2018-05-21 1:06 GMT+02:00 igorpadykov <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Drive 1080p panel on two LVDS channels
reply from igorpadykov
<https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in *i.MX
Community* - View the full discussion
<https://community.nxp.com/message/1016257?commentID=1016257&et=watches.email.thread#comment-1016257>