Hi all,
I am a newbie in iMX platform.
I would like to know about the availability of eMMC NAND flash support in iMX6 BSP.
As per the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf, the MMC Linux driver supports eMMC4.4 SDR and DDR modes.
Does it mean eMMC is supported in accessing NAND flash also?
As per Micron technical document e·MMC Linux Enablement, I understood that a platform specific host layer is needed
in the Linux kernel. Is this layer supported for iMX6 platform controllers in iMX6 BSP?
Thanks,
Honey S
已解决! 转到解答。
Hi Honey,
I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.
eMMC can be connected thru uSDHC I/F and it is supported by our BSP.
Best regards,
Paul
Hi Honey,
I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.
eMMC can be connected thru uSDHC I/F and it is supported by our BSP.
Best regards,
Paul