do you we have rtp library file in mcuxpresso ide(MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13])

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

do you we have rtp library file in mcuxpresso ide(MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13])

516件の閲覧回数
sandeep_c
Contributor I

iam interfacing ip camera with mimxrt1170 processor so i need use rtp protocol so i gone through the sdk but i didnt find the rtp header files so do we have rtp library file in  MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

@MCUXpresso @tcp_ipstack @UDP @Rtpj 

0 件の賞賛
返信
1 返信

498件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sandeep_c ,

   Thank you for your interest in the NXP MIMXRT product.

   About the MIMXRT1170 RTP, you can check the SDK LWIP, it contains the source code:

SDK_2_13_10_MIMXRT1170-EVK\middleware\lwip\contrib\apps\rtp

SDK download link:

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1170-EVK

BTW, in the next time, if you have a question, please use your company email to create the case instead of the 3rd part email, then it will have a higher support level.

Wish it helps you!

Best Regards,

kerry

 

0 件の賞賛
返信