Hello,
Hope you are doing well!
The waveshare 10.5" AMOLED display is booting with suse LINUX 13 full OS whereas when I have connected to i.MX 8M NANO with the 10.5" AMOLED Display the display is not booting up/powering on and getting the error as "Failed to start Terminate Psplash Boot Screen" (image FYR) and when systemctl command is given I found psplash and weston.service being failed(image FYR). guide me to resolve this error and please do also suggest with supported drivers for display with i.MX8M NANO Board.
for more details of the display check the below link
https://www.waveshare.com/10.5inch-HDMI-AMOLED.htm
iMX8M iMX8MNANO
Thanks,
Rohan R E
Thank you for your response.
u-boot > setenv fdt_file imx8mn-ddr4-evk-rm67199.dtb. After setenv, saveenve and boot for this fdt file I am getting unable to read this file(image attached FYR), whereas for u-boot > setenv fdt_file imx8mn-ddr4-evk-rm67191.dtb it is booting up correctly without error but the application is not running on the display. are there any other steps to be followed to run the application? please do let me know.
thanks,
Rohan.R.E
Sanket Parekh