can CCM_CLKo1 of imx6 provide 32.768Khz clock when imx6 is in sleep status?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can CCM_CLKo1 of imx6 provide 32.768Khz clock when imx6 is in sleep status?

Jump to solution
1,541 Views
fangmingan
Contributor I

on our platform , wifi module need  a SLEEP_CLK(32.768K) for low power.

At the beginning, I want to use CCM_CLKO1 to supply this 32.768Khz clock.

But i don't know whether CCM_CLKo1 can still supply 32.768K clock  after  cpu enter sleep status


Labels (1)
0 Kudos
Reply
1 Solution
958 Views
AnsonHuang
NXP Employee
NXP Employee

For sleep state, you mean suspend, right? As all clocks are gated in suspend, although external 32k clock is still there for RTC, but I am afraid you may not get it from CLKO1, you can have a try, if CLKO1 can output 32k in run state but can not in sleep, then I think it is gated. Not very sure about it, better to have a try.

View solution in original post

0 Kudos
Reply
1 Reply
959 Views
AnsonHuang
NXP Employee
NXP Employee

For sleep state, you mean suspend, right? As all clocks are gated in suspend, although external 32k clock is still there for RTC, but I am afraid you may not get it from CLKO1, you can have a try, if CLKO1 can output 32k in run state but can not in sleep, then I think it is gated. Not very sure about it, better to have a try.

0 Kudos
Reply