bitbake core-image-base for mys6ul14x14 error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

bitbake core-image-base for mys6ul14x14 error

跳至解决方案
1,046 次查看
totalit
Contributor III
Having troubles with bitbaking an image of mys6ul14x14. There is Ubuntu 16.04. I cloned a package via "repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth", initialized the environment in ".../sources/poky" using "source oe-init-build-env", set MACHINE=mys6ul14x14, and I get this error on bitbake command:
 
ERROR: ParseError in configuration INHERITs: Could not inherit file classes/fsl-dynamic-packagearch.bbclass
 
Thanks in advance.
0 项奖励
回复
1 解答
996 次查看
totalit
Contributor III

I've successfully completed bitbaking on Ubuntu 20.04 according to i.MX_Yocto_Project_User's_Guide instead of MYS6ULX Linux Development Guide.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
997 次查看
totalit
Contributor III

I've successfully completed bitbaking on Ubuntu 20.04 according to i.MX_Yocto_Project_User's_Guide instead of MYS6ULX Linux Development Guide.

0 项奖励
回复
1,018 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Did you follow i.MX_Yocto_Project_User's_Guide.pdf?

 

0 项奖励
回复
1,008 次查看
totalit
Contributor III

Hey.

Now I'm following i.MX_Yocto_Project_User's_Guide.pdf, previously I was using MYS-6ULX Linux Development Guide and the supplier's packages. The MYS guide is confusing and uncompleted, I'll report when I have positive results.

0 项奖励
回复