bitbake core-image-base for mys6ul14x14 error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake core-image-base for mys6ul14x14 error

ソリューションへジャンプ
1,045件の閲覧回数
totalit
Contributor III
Having troubles with bitbaking an image of mys6ul14x14. There is Ubuntu 16.04. I cloned a package via "repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth", initialized the environment in ".../sources/poky" using "source oe-init-build-env", set MACHINE=mys6ul14x14, and I get this error on bitbake command:
 
ERROR: ParseError in configuration INHERITs: Could not inherit file classes/fsl-dynamic-packagearch.bbclass
 
Thanks in advance.
0 件の賞賛
返信
1 解決策
995件の閲覧回数
totalit
Contributor III

I've successfully completed bitbaking on Ubuntu 20.04 according to i.MX_Yocto_Project_User's_Guide instead of MYS6ULX Linux Development Guide.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
996件の閲覧回数
totalit
Contributor III

I've successfully completed bitbaking on Ubuntu 20.04 according to i.MX_Yocto_Project_User's_Guide instead of MYS6ULX Linux Development Guide.

0 件の賞賛
返信
1,017件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Did you follow i.MX_Yocto_Project_User's_Guide.pdf?

 

0 件の賞賛
返信
1,007件の閲覧回数
totalit
Contributor III

Hey.

Now I'm following i.MX_Yocto_Project_User's_Guide.pdf, previously I was using MYS-6ULX Linux Development Guide and the supplier's packages. The MYS guide is confusing and uncompleted, I'll report when I have positive results.

0 件の賞賛
返信